Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Door Stopper, Lock

Door Stopper, Lock
Sales Price: 13.38 SGD
Review Rating: 4.17
6 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
The door stopper was broken so I used it as a repair part.
4
From Japan
On 2017-07-11 17:49:53
It looks beautiful, and the usability is also quite good. It is not a brand name, but this was enough.
This review is about item#45520596.
I used it for most doors in the house
5
From Japan
On 2016-04-12 17:11:50
There was also a case where alignment including the angle was a little severe again, but the main body was small, it did not become an obstacle, the magnetic force in the state not locked was not strong and weak and it was just right. Since the base cap attached to the floor side is slightly weak, I think it would be better not to come off during cleaning. It is a very good product from the price.
This review is about item#45520596.
On the way in the room, a disturbing place
5
From Japan
On 2015-10-21 06:05:40
I make it firmly for price, I use it without any problem in function.
This review is about item#45520596.
Mansion Doors
2
From Japan
On 2015-02-09 13:12:38
The price satisfaction level is high, but the feeling of stop when opening the door is loose, and if it opens vigorously it will bounce without stopping.
This review is about item#45520596.
door
4
From Japan
On 2014-05-28 20:33:17
I think that there is a problem with the contents of the manual ... · · ·. When laying in for the first time purchased by an amateur, when referring to the product image, it is assumed that it is inside, without knowing at all what it is attached to the inside or the outside of the door, when attaching the flap is released, when using the foot I thought that there was no way to step through with the toes of the toe. . . Even if you search various images on the web, it is difficult to judge whether it is on the inner side, I think that it was kind that you stated "Please install on the outside of the door" in the first section of the manual. People who have never seen · When a person who has never installed has to install it, I do not know the mounting position of the stopper. As for the installation method, it is easy to understand, I think that it is good if there is description only the installation position.
This review is about item#45520596.
Home door
5
From Japan
On 2013-05-23 20:06:11
It is a very good item. I could purchase such a door stopper cheaply, it was good. I think that it will be perfect if the body becomes thinner a little more.
This review is about item#45520596.
1
Customer Who Viewed This Item Also Viewed
Magnet Door Stopper
Magnetic Door Stop, Lock
MG Door Catcher Magnetic Gold
Magne doorstop
Flat doorstop
Metal stopper
TS Catch Lock
Door Stopper