Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Luggage Bag

Luggage Bag
Sales Price: 32.12 SGD
Review Rating: 4.83
6 Customer Reviews
5 star 5
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Organizing cars
5
From Japan
On 2016-03-06 19:17:11
I use it for Hiace. It is very good to be able to effectively use the limited space.
This review is about item#38453581.
Used by hanging on the trunk
5
From Japan
On 2014-10-04 08:16:34
It is very useful. I use small items and use it, but things will not fall, and the fabric seems to be quite okay. If there is another car that can be installed, I would like to purchase again.
This review is about item#38453581.
We are preparing to go on a journey of staying in a car
5
From Japan
On 2014-07-17 16:35:43
It was a product I wanted very much. It's convenient to store what you really need in the back of the seat.
This review is about item#38453581.
It is useful for organizing car trunks
4
From Japan
On 2014-07-14 15:55:49
It is well thought up by the width that is easy to install and also attached to mini vehicles. It is regrettable that a strange odor peculiar to this product will occur, if we wipe it up with water, it got somewhat lost, but the time is going to solve the time (^ _ ^;) the side is slightly narrowed I feel like it does not cause things to fall from the side. It is good that the trunk room of a narrow light car can be easily used widely, even if it is installed, there is no hindrance to the rear seats, for example, there is no hindrance in any way, when removing the full flat it seems better to remove it.
This review is about item#38453581.
Dog, load carrying
5
From Japan
On 2013-03-08 23:22:10
It is attached to the top of a Jimny's hood. Since there is no headrest in the rear seat, it can not be installed behind the rear seat. Since there is no way to put people on the rear seat, we use the front hook and the corner of the ceiling at the rearmost part of the hood and the hook of the product to the metal fittings of the belt coming out from the left and right. (The back seat seating surface, BAG will be on top of 10 ~ 15 cm) There are 8.5 kg of our miniature dachshund, but this BAG has not seemed to break since purchase. Previously I was standing at the rear seat but now I am sleeping longer. I use shopping and wet umbrellas conveniently.
This review is about item#38453581.
Cargo space luggage compartment
5
From Japan
On 2012-02-21 22:56:26
It is attractive that the cargo space which had been frustrating up to now can be afforded even with a refreshing space. Easy to install and satisfied because the material is solid as well.
This review is about item#38453581.
1
Customer Who Viewed This Item Also Viewed
Utility Storage Box
Trunk Net for Car
Car Storage
Console Tray
Door Side Tray
Rope Hook
Multiple Grip Bar
Interior Bar
One-touch holder
Slim Console Caddy
Car Hanger Keeper
Dust Pocket
Headrest Tray
Armrest Pocket