Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Mechanical Pencil for Drafting

Mechanical Pencil for Drafting
Sales Price: 12.51 SGD
Review Rating: 5.00
5 Customer Reviews
5 star 5
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
During drawing
5
From Japan
On 2015-11-18 17:13:50
I also used other manufacturers, but it is said that this manufacturer is nice in the company. It will be appreciated if you can offer it more cheaply. a little expensive.
This review is about item#10438224.
Everyday memo, Machine on site machining Used for use
5
From Japan
On 2015-09-10 23:25:02
It is in active use for in-house processing of machine equipment. It is slightly inconvenient with ordinary pencils (thickness of core point, irregularity), breaking just with 0.5 mm pencil pencil, the same as pencil for 2 mm core for building. . . Of course, I do not want to keep the scribbling needle in my pocket. . . I hit the 0.9 mm core and it felt like "Oh, this one!" Although I love the core of B, 2B, I feel that the taste written in everyday notes is smooth and comfortable. During work I feel "always together".
This review is about item#10438233.
Design draft · rough sketch
5
From Japan
On 2014-07-12 00:08:38
I used ordinary sharpening up to now, but it was good to change this. Easy to hold balance and weight. It is very satisfying with just happy things such as difficult to break the core.
This review is about item#10438215.
I am using it for daily administrative processing, such as to draft at the time of document preparation.
5
From Japan
On 2012-06-05 23:28:16
Although it was only light pencil pen and usability was bad, this product has moderate weight, it is very easy to write. There are many cheap mechanical pens, but they quickly broke, I was looking for good quality items, I tried to buy it because of my recommendation from a friend. Expect great!
This review is about item#10438224.
To ordinary writing
5
From Japan
On 2011-12-12 09:54:16
Since it is not drafting with a drafter this time, I use it for handwritten simple drawings and everyday use. Balance of weight and feeling of nonslip are the best for me. I see other types of things elsewhere, but this is my favorite in Dantotsu.
This review is about item#10438215.
1
Customer Who Viewed This Item Also Viewed
Graph Gear 500
Chart Pencil
Rate Graph
Mechanical Pencils
Drawing Mechanical Pencils
Cutter AL Type
Mechanical Pencil 0.5mm
Mechanical Pencils
Pure Malt Sharp pen
Staedtler drafting pencil