Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of T-Slot Cutter

T-Slot Cutter
Sales Price: 40.03 SGD
Review Rating: 2.86
7 Customer Reviews
5 star 1
4 star 0
3 star 4
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Groove off of stainless steel
1
From Japan
On 2017-10-06 11:32:42
My teeth hung on immediately. I should have bought a better thing even if the price is high
This review is about item#7334756.
Grooving of copper alloy
3
From Japan
On 2014-06-27 14:12:07
It is saved to cheap.
This review is about item#07334756.
Groove digging into the side face of special steel
2
From Japan
On 2014-04-02 13:38:55
The center is crazy. In my own use environment, the frequency of use is low and the grooves to be cut are shallow as much as 1 mm or so, so it does not matter so much, but feelings are not good. The price is cheap, I think that I will use it in the future because it is somehow usable, but I do not want the center to be crazy.
This review is about item#07334756.
Groove on the side
3
From Japan
On 2014-02-12 18:37:24
Delivery was quick, saved. Cutting performance seems to be somewhat lower than the one used before. It is not as bad as it can not be used. I think that it is good to consider the price. Because it is not used frequently, durability is unconfirmed.
This review is about item#07334826.
Correction of locus
3
From Japan
On 2012-11-12 00:21:24
A little sharpness is gentle. Because it is only the bottom use, it is different from the original use.
This review is about item#07334826.
Aluminum T slot Miso processing
5
From Japan
On 2011-01-05 02:48:17
Sharpness and dimensions are unchanged with other companies, price and instant delivery are attractive, but this time the 13 x t 3 orders were 13 x t 4 in kind. The notation on the top and the side of the box was different. For the order of 10 × t 2 before, the actual thing was 10 × t 3. Although it was usable this time, it is a bit uneasy from now on.
This review is about item#07334774.
Groove processing
3
From Japan
On 2007-12-11 14:10:30
It is good for T grooving so it is cheap because it is a necessary item.
This review is about item#07334756.
1
Customer Who Viewed This Item Also Viewed
Angle Shank Type Chamfering Cutter
Key sheet cutter
Key sheet cutter
T slot end mill
T Slot Cutter
Staggered blade T slot cutter
Long Shank T-slot cutter
T Slot Cutter
Chidori blade T-slot cutter
T Slot Cutter